Example for the DMAFromPC Operator on the imaFlex CXP-12 Quad Platform

Brief Description

Files: examples\Processing\Shading\Shading2D\DMAFromPC\DMAFromPC.vad

Default Platform: imaFlex CXP-12 Quad

Short Description

Demonstration of the functionality of the DMAFromPC operator.

This example demonstrates how you can use the DMAFromPC operator on an imaFlex CXP-12 Quad platform to transfer images from the PC to the frame grabber using the example of shading correction. See the Framegrabber SDK example script, which you can find in the same directory as the *.va file, to see how the DMAFromPC functionality can be used during runtime.